Flip graphic objects

Use the Flip Vertical or Flip Horizontal options on the Arrange menu to move an object so its new position is a mirror image of its original position. You can flip group and simple objects.
Flip Vertical turns an object upside down. Flip Horizontal switches the object from left to right.
Flipping_Objects_Vertically
Flipping_Objects_Horizontally
To flip an object:
  1. In a graphic display, click the object to be repositioned to select it.
  2. Click
    Arrange
    >
    Flip Vertical
    or
    Flip Horizontal
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal