Bring a graphic object to the front

Graphic objects can be stacked on top of each other in a graphic display. Use the Bring to Front option on the Arrange menu to move the selected object to the top of the stack.
Stacking-Objects2
To bring a graphic object to the front:
  1. In a graphic display, click an object to select it.
  2. Click
    Arrange
    >
    Bring to Front
    .
To select the object at the back:
  • Click the top object once, pause, and then click again. Do not double-click, and do not move the mouse.
You can select several objects with a selection border and move them simultaneously but as individual objects, or group objects and move them as a single object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal