Send a graphic object to the back
Graphic objects can be stacked on top of each other in a graphic display. Use the Send to Back option on the Arrange menu to move the selected object to the bottom of the stack.

To send a graphic object to the back:
- In a graphic display, click an object to select it.
- ClickArrange>Send to Back.
To select the object at the back:
- Click the top object once, pause, and then click again. Do not double-click, and do not move the mouse.
You can either select several objects with a selection border and move them simultaneously but as individual objects, or group objects and move them as a single object.
Provide Feedback