Arrange options
The following table shows options on the
Arrange
menu.This option | Description |
---|---|
Group | Combines several objects into a group that behaves as a single object. |
Ungroup | Divides an object into its components parts. |
Send to Back | Stacks objects by moving them behind other objects. |
Bring to Front | Stacks objects by moving them in front of other objects. |
Align Left | Aligns objects to left-most selected object. |
Align Right | Aligns objects to right-most selected object. |
Align Center | Aligns objects to horizontal center of all selected objects. |
Align Top | Aligns objects to top-most selected object. |
Align Middle | Aligns objects to vertical center of all selected objects. |
Align Bottom | Aligns objects to bottom-most selected object. |
Align Center Points | Aligns objects to center of all selected objects. |
Align to Grid | Aligns objects to grid. |
Space Vertical | Spaces objects vertically. |
Space Horizontal | Spaces objects horizontally. |
Flip Vertical | Flips objects vertically. |
Flip Horizontal | Flips objects horizontally. |
Provide Feedback