Edit a display
You can use the menu or toolbar options to edit an existing graphic display.
To edit a graphic display:
- InFactoryTalk View Studio, in theGraphicseditor, in theExplorewindow, expandGraphics>Displays.
- Double-click the display you want to edit. You can also right-click it and selectOpen.
- Use the tools and menu options available in theGraphicseditor to modify the graphic display.
- Save the graphic display. If you are editing a graphic template as the basis for a new graphic display, clickSave Asto give the graphic display a new name. All graphic displays are given the extension .gfx when you save them.TIP:To see the menu options available for any object in the graphic display, click the right mouse button when the cursor arrow is pointing at the object. This displays a context menu. To select a command from the menu, click it or highlight it then press Enter.To edit an embedded object that was not created by the Graphics editor you can use in-place editing to do so without leaving the Graphics editor.
Provide Feedback