About the context menu

The context menu is displayed when you click the right mouse button. The items displayed on the menu depend on the object the mouse pointer is positioned over when the button is pressed.
To select a command from the menu, click it or highlight it then press Enter. To close the menu, click anywhere outside it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal