About in-place editing

In-place editing lets you edit an embedded object without leaving the graphics display.
To do this, select and then double-click the object. This activates the source application, replacing the Graphic Displays bar menu with the bar menu for the source application and allowing you to make changes to the object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal