Align graphic objects

Use the
Align
option on the Arrange menu to position selected objects so that they line up with each other and the grid. Final positioning depends on the commands used.
To align graphic objects:
  1. In the graphic display, hold the
    Ctrl
    key, click the objects you are going to align.
  2. On the
    Arrange
    menu, select an alignment option to arrange the selected objects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal