Move a graphic object

You can move several objects at once by selecting them all and dragging one of the selected objects. When you are moving the selected objects, they are displayed in outline form. You can also move an object in small increments.
TIP:
You can also use Cut and Paste to move objects in a graphic.
To drag an object with the mouse:
  1. Select the object or objects.
  2. Place the pointer on the object, not on its edge or handle.
  3. Press the mouse button and drag the object to its new location.
To move an object in small increments:
  1. Select the object or objects.
  2. Place the pointer on the object, not on its edge or handle.
  3. Press an arrow key.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal