Space graphic objects equidistantly
Use the
Space Vertical
and Space Horizontal
options on the Arrange
menu to move selected objects so there is an equal amount of space between them. You must select at least three objects to use either of these commands.
To space objects equidistant from each other:
- In a graphic display, select at least three objects.
- ClickArrange>Space VerticalorSpace Horizontalto align the objects.TIP:Space Verticalshifts objects so their center points are same vertical distance from one another. The top and bottom objects do not move, but the other objects move up or down so there is equal space between the center of each object and those above and below it.Space Horizontalshifts objects so the center points of each object are the same horizontal distance from one another.To arrange objects in a column, arrange them roughly, and then select them and useAlign Centerand thenSpace Verticalto arrange them exactly. For a horizontal line, useAlign Middleand thenSpace Horizontal.
Provide Feedback