Security Policy Properties
How do I open Security Policy Properties?
In the
Explorer
window, expand System
> Policies
> System Policies
and double-click Security Policy
.Use
Security Policy Properties
to define general rules for implementing security across all FactoryTalk
products in the system. To modify security policies, obtain the appropriate permissions for the System Policies
folder in the Explorer
.- Account Policy Settings: Specifies howFactoryTalkmanages policies for user, computer, and group accounts.
- Badge Policy Settings: Specifies howFactoryTalkuser accounts can log on using a Radio-Frequency-Identification (RFID) badge.
- Computer Policy Settings: Specifies how computer accounts in theFactoryTalknetwork directory can use remote access.
- Directory Protection Policy Settings: Specifies client computer accounts usage of theFactoryTalknetwork directory.
- DNS Alias Name: Specifies a DNS alias name associated with a computer hosting theFactoryTalk Directoryserver.
- Encryption Settings: Specifies the encryption and decryption algorithm used by FactoryTalk products.
- System Communication Settings: Specifies the communication settings in the FactoryTalk event system.
- Password Policy Settings: Specifies password requirements forFactoryTalkuser accounts.
- Service Token:Specifies whether to use a signed service token.
- Single Sign-On Policy Settings: Specifies whether users can log on once to theFactoryTalksystem or must log on to eachFactoryTalkproduct separately.
- Web Authentication Settings: Specifies the Microsoft Entra ID (as known as Azure AD) user sign-in settings.
- Web Authentication/Authorization Server: Specifies security settings for FactoryTalk-enabled software web applications.
Provide Feedback