Disable single sign-on

To require users to log into each
FactoryTalk
product separately, configure
Single Sign-On Policy Settings
to disable single sign-on capability.
To disable single sign-on
  1. In
    FactoryTalk Administration Console
    Explorer
    , expand
    System > Policies > System Policies
    .
  2. Right-click
    Security Policy
    and select
    Properties
    .
  3. In
    Security Policy Properties
    , select
    >
    to expand
    Single Sign-On Policy Settings
    .
  4. To the right of
    Use single sign-on,
    select the down arrow.
  5. Choose
    Disabled
    , then select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal