Web Authentication Settings

Web Authentication Settings
are only available for the Microsoft Entra ID user sign-in.
Setting
Description
Web authentication timeout
Specifies the amount of time before the connection is timed out. The value ranges from 15 through 3600.
Web authentication retry counts
Specifies the connection retry counts. The value ranges from 1 through 100.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal