Modify Web Authentication Settings

Use
Web Authentication Settings
to specify the Microsoft Entra ID user sign-in settings.
To modify Web Authentication Settings
  1. In the FactoryTalk Administration Console
    Explorer
    pane, go to
    System
    >
    Policies
    >
    System Policies
    .
  2. Double-click
    Security Policy
    .
  3. Under
    Web Authentication Settings
    , configure:
    • Web authentication timeout
      Specifies the amount of time before the connection is timed out. The value ranges from 15 through 3600.
    • Web authentication retry counts
      Specifies the connection retry counts. The value ranges from 1 through 100.
  4. Select
    OK
    or
    Apply
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal