Modify Computer Policy Settings

Use
Computer Policy Settings
to change these security policy properties:
  • Whether or not a user can connect to the
    FactoryTalk Directory
    from a client computer that does not have a computer account in the network directory
  • How client computers connect to the
    FactoryTalk Directory
    through Remote Desktop Services, and how the computer name appears in the
    FactoryTalk Diagnostics
    log of actions.
These settings apply only to computers in the
FactoryTalk
network directory because the
FactoryTalk
local directory does not permit remote access.
To modify Computer Policy Settings
  1. In
    FactoryTalk Administration Console
    Explorer
    , expand
    System > Policies > System Policies
    .
  2. Right-click
    Security Policy
    and select
    Properties
    .
  3. In
    Security Policy Properties
    , select
    +
    to expand
    Computer Policy Settings
    .
  4. To change the requirements for connecting to the
    FactoryTalk Directory
    from a computer that does not have a
    FactoryTalk
    computer account, select
    Require computer accounts for all client machines
    and select one:
    • Enabled—
      allows users to log on to
      FactoryTalk
      only if they are logging on from a client computer that has an account in the
      FactoryTalk Directory
      . Remote Desktop Services clients can still log on to
      FactoryTalk Directory
      without computer accounts if the
      Identify terminal server clients using the name of
      policy is set to
      Server Computer
      . See step 4.
    • Disabled—
      allows users to log on to
      FactoryTalk
      from any client computer, even if that computer has no computer account in the
      FactoryTalk
      network directory.
  5. To determine what computer name identifies clients connecting to the
    FactoryTalk Directory
    through Remote Desktop Services, select
    Identify terminal server clients using the name of
    and select one:
    • Terminal client
      —Client computers must have computer accounts in the
      FactoryTalk Directory
      to access
      FactoryTalk
      applications, unless the
      Require computer accounts for all client machines
      policy is disabled. This combination of settings is useful for diagnostic logging because the name of the client computer where actions originate can be logged.
      Terminal Client
      logs actions using the name of the client computer where the user is connecting to the Remote Desktop Connection (RDC) client computer. The computer name logged in
      FactoryTalk Diagnostics
      is different for each client connecting via Remote Desktop Services.
    • Server computer—
      allows client computers to connect through Remote Desktop Services without requiring accounts in the
      FactoryTalk Directory
      , even if the
      Require computer accounts for all client machines
      policy is
      Enabled
      .
      Server computer
      logs actions using the name of the Remote Desktop Connection server computer. The computer name logged in
      FactoryTalk Diagnostics
      will be the same for all users connecting via Remote Desktop Services.
  6. To determines if the system will force the use of the local computer name when a disconnected remote session is blocking the logon process, select
    Force use of local computer name during logon process
    and select one:
    • Enabled—
      allows using the local computer name to log in if the remote session is disconnected.
    • Disabled—
      does not allow logging in to the
      FactoryTalk Directory
      if the remote session is disconnected.
  7. When finished modifying Account Policy Settings, select
    OK
    .
    IMPORTANT:
    Setting the
    Identify terminal server clients using the name of
    policy to
    Server Computer
    might affect the level of access that a Remote Desktop Services user has to the
    FactoryTalk
    system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal