Computer Policy Settings
Computer Policy Settings
control how computer accounts can access the FactoryTalk Directory
remotely. These settings apply only to computer accounts in the FactoryTalk
network directory because the FactoryTalk
local directory does not permit remote access.Setting | Description |
---|---|
Require computer accounts for all client machines | Determines whether client computers can access the FactoryTalk network directory without having a computer account in the network directory. Disable this policy to allow users to connect remotely from any computer, even if the computer does not have a computer account in the FactoryTalk Directory .Even when this setting is disabled, create computer accounts for any computers hosting servers — for example, Rockwell Automation Device Servers (FactoryTalk Linx , OPC data servers, Tag Alarm and Event Servers, or HMI servers. Without the server computer accounts, configuring the servers from client computers on the network is not possible. The FactoryTalk network directory Server cannot locate these servers on the network without their computer accounts.Enabled allows users to log on to FactoryTalk only if they are logging on from a client computer that has an account in the FactoryTalk Directory . Even if set to Enabled, Remote Desktop Services clients can still log on to FactoryTalk Directory without computer accounts if the Identify terminal server clients using the name of policy is set to Server Computer .Disabled allows users to log on to FactoryTalk from any client computer, even if that computer has no computer account in the FactoryTalk network directory.Default : Enabled |
Identify terminal server clients using the name of | Determines what computer name identifies clients connecting to the FactoryTalk Directory through Remote Desktop Services. This policy also affects whether client computers connecting through Remote Desktop Services require computer accounts in the FactoryTalk Directory .Server Computer allows client computers to connect through Remote Desktop Services without requiring accounts in the FactoryTalk Directory , even if the Require computer accounts for all client machines policy is Enabled . This is possible because the FactoryTalk Directory behaves as if the client computer were accessing the FactoryTalk Directory from the Remote Desktop Connection computer.If set to Terminal Client and the Require computer accounts for all client machines policy is Enabled , client computers must have computer accounts in the FactoryTalk Directory to access FactoryTalk applications.If set to Terminal Client and the Require computer accounts for all client machines policy is Disabled , client computers do not require computer accounts in the FactoryTalk Directory to access FactoryTalk applications. This combination of settings is useful for diagnostic logging because the name of the client computer where actions originate can be logged.The Identify terminal server clients using the name of policy also determines which computer name appears in the FactoryTalk Diagnostics Log of actions performed on the system over a Remote Desktop Services connection:Terminal Client logs actions using the name of the client computer where the user is connecting to the Terminal Server. The computer name logged in FactoryTalk Diagnostics will be different for each client connecting via Remote Desktop Services.Server Computer logs actions using the name of the Terminal Server computer for all users. The computer name logged in FactoryTalk Diagnostics will be the same for all users connecting via Remote Desktop Services.Default : Terminal Client |
Force use of local computer name during logon process | Determines if the system will force the use of the local computer name when a disconnected remote session is blocking the logon process. Enabled allows using the local computer name to log in if the remote session is disconnected.Disabled does not allow logging in to the FactoryTalk Directory if the remote session is disconnected.Default : Disabled |
IMPORTANT:
Setting the
Identify terminal server clients using the name of
policy to Server Computer
might affect the level of access that a Remote Desktop Services user has to the FactoryTalk
system. Provide Feedback