Single Sign-On Policy Settings

Use
Single Sign-On Policy Settings
in
Security Policy Properties
to set whether users can log on once to the
FactoryTalk
system or must log on to each
FactoryTalk
product separately.
Disable single sign-on if users will be connecting through Remote Desktop Services using the name of the Remote Desktop Connection server computer. This is determined through the computer policy setting
Identify terminal server clients using the name of.
The computer name is saved as part of the single sign-on user's credentials and might affect the level of access a user has to the
FactoryTalk
system.
Setting
Description
Enabled
Requires users to log on to the
FactoryTalk
system only once. The system checks the user's access rights as the user performs actions after logging on. If the user has the required access rights, the action is allowed to proceed. If the user does not have the required access rights, the action is prevented from taking place. The user is not prompted repeatedly to log on with a user name and password.
Disabled
Requires users to log on to each
FactoryTalk
product separately.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal