Configure a site binding
The site binding configuration will affect all computers using the FactoryTalk Reverse Proxy.
To configure a site binding
- On the FactoryTalk Directory server computer, open FactoryTalk Administration Console.
- In theExplorerpane, go tolocalhost > System > Policies > System Policies > Security Policy.
- ChangeReverse Proxy PortandReverse Proxy Protocolas needed.IMPORTANT:
- Ensure that the reverse proxy port is allowed through the computer’s firewall, for example, Windows Defender Firewall.
- IfReverse Proxy PortorReverse Proxy Protocolchanges, the FactoryTalk system will make changes toSite Bindingsin the Internet Information Services (IIS)Default Web Site. You may need to reconfigure the certificate if you have HTTPS enabled.
- If you want to use HTTPS only, remove the binding of HTTP with port 80 in IIS after installation.
- SelectApply, and then selectOK.
Provide Feedback