Modify Service Token

Use
Service token
to specify whether to use a signed service token.
To modify Service Token
  1. In the FactoryTalk Administration Console
    Explorer
    , go to
    System
    >
    Policies
    >
    System Policies
    .
  2. Double-click
    Security Policy
    .
  3. Under
    Service token
    , select
    Service token signature method
    , and then select:
    • Legacy:
      The legacy method ensure compatibility with version 6.31.00 or earlier FactoryTalk Directory clients.
    • Enhanced:
      The enhanced method increases the security of communications using the signature service token.
      When selecting Enhanced, only version 6.40.00 and later FactoryTalk Directory clients can successfully communicate using the service token.
    After changing the setting, you must restart the FactoryTalk system.
  4. Select
    OK
    or
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal