Modify Web Authentication/Authorization Server

Use
Web Authentication/Authorization Server
to set security policies for FactoryTalk-enabled software web applications.
To modify Web Authentication/Authorization Server
  1. In the
    FactoryTalk Administration Console
    Explorer
    pane, go to
    localhost > System > Policies > System Policies
    .
  2. Double-click
    Security Policy
    .
  3. In
    FactoryTalk Web Authentication port
    , enter a port number for the FactoryTalk-enabled software web applications.
    The default port is 7110.
  4. In
    FactoryTalk Web Support Service port
    , enter a port number for the FactoryTalk Web Support Service.
    The default port is 7111.
  5. In
    Reverse Proxy port
    , enter the website port number for computers using the FactoryTalk Reverse Proxy Server.
    If you are using HTTPS, the default port is 443.
    If you are using HTTP, the default port is 80.
  6. In
    Reverse Proxy port
    , select
    HTTPS
    or
    HTTP
    .
    If
    Reverse Proxy port
    or
    Reverse Proxy protocol
    is changed, the system will make changes to
    Site Bindings
    in the Internet Information Services (IIS)
    Default Web Site
    . If you use HTTPS to secure the communication, you may need to reconfigure the certificate for the HTTPS site binding.
  7. In
    Access token expiration
    , enter a value from 1 through 525,600 to change the amount of time before the access token expires.
  8. In
    Authorization code expiration
    , enter a value from 1 through 1,440 to change the amount of time before the authorization code expires.
  9. In
    Refresh token expiration
    , enter a value from 1 through 1,440 to change the amount of time before the refresh token expires.
  10. Select
    Apply
    , and then select
    OK
    .
    Restart the computer to apply the configuration changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal