Web Authentication/Authorization Server

The following table shows the security settings for FactoryTalk-enabled software web applications.
Setting
Description
FactoryTalk Web Authentication port
Specifies the communication port that FactoryTalk-enabled software web applications can access. The default port is 7110.
FactoryTalk Web Support Service port
Specifies the communication port that the FactoryTalk Web Support Service can access. The default port is 7111.
Reverse Proxy port
Specifies the website port for computers using the FactoryTalk Reverse Proxy Server.
  • If you are using HTTPS, the default port is 443.
  • If you are using HTTP, the default port is 80.
Reverse Proxy protocol
Specifies the communication protocol, HTTPS or HTTP, for computers using the FactoryTalk Reverse Proxy Server.
Access token expiration
Specifies the amount of time before the access token expires.
  • Minimum:
    1 minute
  • Maximum:
    525,600 minutes
  • Default
    :
    60 minutes
Authorization code expiration
Specifies the amount of time before the authorization code expires.
  • Minimum:
    1 minute
  • Maximum:
    1,440 minutes
  • Default
    :
    10 minutes
Refresh token expiration
Specifies the amount of time before the refresh token expires.
  • Minimum:
    1 minute
  • Maximum:
    1,440 minutes
  • Default
    :
    1,440 minutes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal