Modify Encryption Settings

Use
Encryption Settings
to specify the encryption and decryption algorithm used by FactoryTalk products.
To modify Encryption Settings
  1. In the FactoryTalk Administration Console
    Explorer
    , go to
    System
    >
    Policies
    >
    System Policies
    .
  2. Double-click
    Security Policy
    .
  3. In
    Encryption Method
    , select:
    • Legacy:
      Uses the legacy encryption algorithm to ensure compatibility with FactoryTalk Services Platform version 6.31.00 and earlier.
    • Enhanced:
      Uses the enhanced encryption algorithm to meet modern security requirements for the FactoryTalk system.
    If
    Enhanced
    is selected, all clients must be upgraded.
  4. Select
    OK
    or
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal