- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Scroll view
Panel with the possibility of scrolling, to display content larger than the panel itself
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Enables zoom | Zoommable | Enable pinch-to-zoom | |
Maximum zoom in | MaxZoomIn | Magnification limit in percent | |
Minimum zoom out | MinZoomOut | Shrinkage limit in percent | |
Scroll axes enabled | ScrollAxesEnabled | Axes for which scrolling is enabled | |
MoveTarget | |||
ScrollBar style | ScrollBarStyle | Style for scrollbars | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Provide Feedback