Add a trend pen toggle
    Add a switch or checkbox that toggles the visibility of a trend pen.
Prerequisites
- To add a trend pen toggle
 - Create a Boolean variable. See Create a variable.
 - Select theSwitchobject and create a dynamic link betweenCheckedand the Boolean variable. See Create dynamic links.
 - Select theTrendobject, and under the desiredTrendPen#, create a dynamic link betweenEnabledand the Boolean variable. See Create dynamic links.
 
Provide Feedback