- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Option button
Selects a mutually exclusive option in a group of options
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Text | Text | Text inserted and displayed | |
Word wrap | WordWrap | Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set | |
Text trimming | Elide | Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set | |
Checked | Checked | Interrupter status. To enable another interface object when the value is True, create a dynamic link between this property and the Enabled property of the object to be enabled | |
Indicator position | IndicatorPosition | Position of the button relative to the text | |
Font family | FontFamily | Font family | |
Font weight | FontWeight | Font weight | |
Font italic | FontItalic | Enables/disables italics in the text | |
Font size | FontSize | Font size | |
Text color | TextColor | Color of the text to display | |
Style | Style | Graphic style applied to the control | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Events
Modified value
- BrowseName
Event that is triggered when the user changes the value of the control
Provide Feedback