- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Pie chart
Display model or database data in a pie chart
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Model | Model | Reference to the information model or database from which to obtain the data | |
Query | Query | Standard SQL query to filter the data of interest. You can use it to filter data from a database and to filter data obtained from a node-based model. In case of a node-based model, the SELECT * FROM Model part is mandatory, followed by the WHERE clause with which to indicate the search conditions - for example, SELECT * FROM Model WHERE Speed > 40 | |
Label | Label | Chart section labels | |
Value | Value | Value displayed and possibly changed by the user | |
Style | Style | Graphic style applied to the control | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Methods
Refresh
- BrowseName
- Refresh
Refresh the displayed data
Provide Feedback