Navigate a trend chart
    Navigate the X-axis and Y-axis of a trend chart in the 
Normal
 trend mode.- Select a point and drag it horizontally to navigate the X-axis.TIP: If theFollowproperty is set toTrue, automatic scrolling stops when you interact with the graph. To restart the automatic scrolling of the X-axis, scroll the X-axis to the current instance.
 - Select a point and drag it vertically to navigate the Y-axis.
 - Select a pointer and drag it diagonally to browse on both axes.
 
Provide Feedback