Draw an oval or circle
    Use the 
Ellipse
 tool to draw and oval or circle.- InProject view, double-click the container to include the object.
 - In the editor toolbar, selectEllipse.
 - In the editor, position the crosshair where the oval or circle is to begin.
 - Drag to draw the oval or circle.
 
The object appears in the editor and in 
Project view
.Provide Feedback