Draw a rectangle or square
    Use the 
Rectangle
 tool to draw rectangles or squares.- InProject view, double-click the container to include the object.
 - In the editor toolbar, selectRectangle.
 - In the editor, position the crosshair where the square or rectangle is to begin.
 - Drag to draw a rectangle or square.
 
The object appears in the editor and in 
Project view
.Provide Feedback