Create an event logger
    Create a logger that monitors the current temperature.
- InProject view, right-clickLoggersand select .
 - Configure events:
- InProperties, next toEvent configurations, select.

 - SetListen subtreetoFalse.
 - Set theEvent typetoAlarmConditionType.
 - InProperties, double-clickEventLogger1
 - In the central pane, select these variables:
- .
 - .
 - .
 - .
 - .
 - .
 
 - In the central pane, selectApply.
 
 - Create a dynamic link betweenDatabaseand .For more information about dynamic links, see Create dynamic links.
 
Provide Feedback