Add users
    Add users with different locales.
Prerequisites
Add the it-IT locale. See Add a locale language to a localization dictionary.
- To add users
 - InProject viewpane, expandSecurity.
 - Create two users by right-clickingUsersand selecting .
 - Rename the users by hovering-over each user, selecting, and entering:

- Alice
 - Jeremy
 
 - InProject view, selectAlice.
 - InProperties, set theLocaleproperty value toit-IT.
 
Provide Feedback