Create a variable
    Create a variable that indicates the current temperature.
- Create the variable:
- InProject view, right-clickModeland select .
 - Hover-over the variable, select, and enter
Temperature. 
 - Configure the variable:
- InProperties, selectInt32and selectFloat.
 - Right-clickTemperatureand select .
 - UnderEURange, setHigh limitto100.
 
 
Provide Feedback