Configure an XY chart
    Configure an XY chart to visualize data.
- InProject view, inUI, right-click a container and then select .
 - (optional) InProperties, set:
- Zoom. The zoom level of the chart.
 - Center X. X coordinate in relation to which to center the chart.
 - Center Y. Y coordinate in relation to which to center the chart.
 - Key visible. Show or hide the legend of the pens.
 
 
Do any of these:
        
Provide Feedback