FactoryTalk AssetCentre Disaster Recovery Capability
The FactoryTalk AssetCentre Disaster Recovery capability allows users to configure the FactoryTalk AssetCentre system to upload the program files from their assets at scheduled intervals. These files can then be checked into the FactoryTalk AssetCentre Archive, and/or compared to a last known good version to generate a difference report.
Disaster Recovery is available with the following capability options:
- Disaster Recovery for Rockwell Automation
- Disaster Recovery for Fanuc robots
- Disaster Recovery for Motoman robots
- Disaster Recovery for ABB robots
- Disaster Recovery for Remote Computers
- Disaster Recovery for Generic FTP
- Disaster Recovery for Custom Devices
- Disaster Recovery for Asset Inventory
- Disaster Recovery for Siemens S7 Controller (STEP7)
- Disaster Recovery for Siemens S7 Controller (TIA Portal)
- Disaster Recovery for Mitsubishi Controller (GX Works2)
- Disaster Recovery for Mitsubishi Controller (GX Works3)
- Disaster Recovery for Schneider Controller (Control Expert)
Refer to Knowledgebase Document ID: QA29309 – FactoryTalk AssetCentre Disaster Recovery Device Support.
Provide Feedback