Generic FTP Device Compatibility

When performing backups or backup and compares on Generic FTP devices containing subdirectories, the FTP device must support both the “DIR” and “ls” commands. Identical directory listings should be displayed for each command, though the format will differ.
TIP:
If no user account is specified, the anonymous account will be used for FTP access. Refer to Knowledgebase Document ID: QA20349 - What user account does the Generic FTP Device use when there is no password set
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal