ControlLogix Change Detect Scheduled Task Creation
As of v4.10, the Change Detect scheduled task is available in FactoryTalk AssetCentre. Creating this schedule will automatically add any available v20 or higher ControlLogix asset from the point of creation in the asset tree. There is no time property for this task; once enabled, it will run all of the time. Therefore, there is no resource-driven reason to break apart the asset tree into separate Change Detect scheduled tasks. It is recommended to create the Change Detect schedule at the root AssetCentre node of the asset tree.
TIP:
Backup and Backup & Compare operations will run normally while the Change Detect scheduled task is running. Monitoring the same device that is being backed up is fully supported.
Provide Feedback