Asset Inventory Management with CIP Devices
Asset Inventory CIP scanning uses an RSLinx Classic driver, meaning that only Rockwell Automation assets will be returned as part of the CIP scan (e.g., no Siemens devices would be discovered). The timeouts associated with CIP scanning in the advanced properties of the asset correspond to how long AssetCentre will wait for an initial CIP response, then how long to wait for a response for the CIP information. It is recommended that these timeouts be left at the default values.
Provide Feedback