Asset Inventory Management Disaster Recovery Schedules

Disaster Recovery for Asset Inventory allows the user to schedule FactoryTalk AssetCentre to browse the network for CIP, SNMP, and/or WMI assets. These assets are collected into an RAAI file, which is stored in the AssetCentre archive. The RAAI file can be viewed within the AssetCentre desktop client, and can be used to add/update the AssetCentre asset tree.
Because the network scan can take much more time than backing up an individual asset, it is recommended that each Asset Inventory asset be configured in an independent Disaster Recovery schedule.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal