Asset Inventory Management with SNMP Devices
Asset Inventory SNMP scanning will browse the identified address range, ping each individual address to determine if it is available, and then send an SNMP get-request. If the device responds, the AssetCentre service will request all available SNMP information. Note that the community string can only be set globally, not on a per-device level.
The Asset Inventory scan uses SNMP version 2.0. Some properties can be returned from devices using v1.0 of SNMP, but v3.0 is not supported.
Provide Feedback