Disaster Recovery with ControlLogix Source Protection
Source Protection is supported with Disaster Recovery. If the source key is configured within the ACD file, the Logix Designer Compare Utility will compare the source protected contents. The source key path must be configured in the ACD file when logged in as the user configured to run the VerificationAgent service, and the key file must be available on each AssetCentre Agent. For more information, refer to Knowledgebase Document ID: QA39453 – FactoryTalk AssetCentre Disaster Recovery with Logix Designer Source Protection.
Provide Feedback