Using Disaster Recovery for Remote Computers on Locked Files
Files that are locked and/or in use when a Remote Computer schedule is run cannot be backed up by the FactoryTalk AssetCentre agent. For instance, a FactoryTalk View SE server that is currently being used in product will have its files locked, meaning that the FactoryTalk AssetCentre agent cannot back up a running View SE HMI server. For more information, see Knowledgebase Document ID: IN28481 - Backing up Locked Files with FactoryTalk AssetCentre.
Provide Feedback