Disaster Recovery with the FactoryTalk Directory
As of version 8.00 of FactoryTalk AssetCentre, a FactoryTalk Directory asset is available for Disaster Recovery operations. The FactoryTalk Directory asset uses FactoryTalk Security credentials to log into the directory, and is capable of backing up specific applications (hierarchy only) or the entire directory, including security configurations. FactoryTalk Directory assets are scheduled as part of Disaster Recovery for Rockwell Automation tasks.
TIP:
A FactoryTalk Directory backup will always return differences. Version control should be monitored to prevent a large number of versions.
Provide Feedback