About Options dialog boxes
With the
Options
dialog boxes, you can specify some overall settings regarding the display and action of the FactoryTalk AssetCentre desktop client on this computer. For example, set the refresh rate for the Logs tab or specify a software program that the Archive component should use to open files with a certain extension.The
Options
dialog boxes include:- Options dialog box: Archive Options
- Options dialog box: Asset Inventory
- Options dialog box: Assets Lifecycle
- Options dialog box: Change Detect
- Options dialog box: Compare Configuration
- Options dialog box: Compare Engines
- Options dialog box: Custom Devices
- Options dialog box: Database Limitations
- Options dialog box: Database Maintenance
- Options dialog box: Extended Properties
- Options dialog box: File Associations
- Options dialog box: Log Viewer
- Options dialog box: Scheduled Operations
- Options dialog box: Stratix Switch
Provide Feedback