Options dialog box: Log Viewer

How do I open the Options: Log Viewer dialog box?
  1. Select
    Tools > Options
    .
  2. Under
    Category
    on the left side of the dialog box, select
    Logs Viewer
    .
Use the
Options: Log Viewer
dialog box to set log view options, including:
  • Refresh Rate
    Enter the time interval, from 5 to 60 seconds, at which all logs should be refreshed.
  • Row display options
    Enter the number of rows (between 1 and 500) to show for each of the logs:
    • Event
      Enter the maximum number of rows to show in the Event Log.
    • Audit
      Enter the maximum number of rows to show in the Audit Log.
    • Diagnostic/Health
      Enter the maximum number of rows to show in the Diagnostics and Health Log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal