Change the refresh rate and number of shown records
Set the maximum number of records and refresh rate for shown logs.
Prerequisites
- To set log options, you must haveView Event Log,View Audit Log, orView Diagnostics and Health Logpermissions.
To change log options
- SelectTools > Options.
- UnderCategoryon the left side of the dialog box, selectLog Viewer.
- Complete theOptions dialog box: Log Viewer.
- ClickOK.
Provide Feedback