Configure security for FactoryTalk AssetCentre

By default, the Administrators and All Users groups in FactoryTalk Directory can perform any task in the FactoryTalk AssetCentre software. To deny specific users the right to perform tasks in FactoryTalk AssetCentre, you must edit the Feature Security settings in the FactoryTalk Administration Console.
IMPORTANT:
Never explicitly deny rights to the All Users or Administrators group in FactoryTalk. Rather, set up specific user groups of your own and deny rights to those groups. Denying rights to All Users or Administrators could lock everyone out of the system and would deny rights in all FactoryTalk-enabled products.
To configure security for FactoryTalk AssetCentre
  1. Select
    Start
    >
    Rockwell Software
    >
    FactoryTalk Administration Console
    .
  2. In the Explorer pane, navigate to
    System
    >
    Policies
    >
    Product Policies
    >
    FactoryTalk AssetCentre
    .
  3. Double-click
    Feature Security
    .
  4. Click the feature (policy setting) for which you want to set permissions. Click the browse button browse_button_small next to the words Configure Security.
  5. In the
    Configure Securable Action
    dialog box, select the user or group for whom you want to assign permissions. (If the user or group does not appear in the list, click
    Add
    , click
    Show all
    , select the user or group, and click
    OK
    .)
  6. Click the box to allow or deny the user permission to the selected feature.
  7. Click
    OK
    .
    IMPORTANT:
    Do not use the Server Settings properties in the FactoryTalk Administration Console to change server settings. Instead go to
    Start
    >
    Rockwell Software
    >
    FactoryTalk AssetCentre Server Settings
    on the server computer. Changing server settings in the FactoryTalk Administration Console could enter conflicting information and prevent clients from connecting to the server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal