Change server settings

You will change server settings only under rare circumstances, such as if a client can't connect to server.
To change server settings
  1. On the server computer, select
    Start > Rockwell Software > FactoryTalk AssetCentre Server Settings
    .
  2. If you are not logged in to FactoryTalk, you will be asked to do so.
  3. Fill out the fields on the
    Configure Server Settings Utility
    . Click
    Help
    in the dialog box for information on any of the fields.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal