Change security settings for an asset
Each asset in the asset tree has security settings controlling which users can perform what actions with that asset.
Prerequisites
To change security settings for an asset, you must have the following permissions:
- Switch to Design mode
- Configure Security
To change security settings for an asset
- Switch to Design mode.
- Right-click the asset in the Asset View and selectSecurity, or select an asset and then select
in the Asset View. - On thePermissionstab, select whether you want to set permissions byUseror byAction.
- In the top pane select the user or the action for which you want to set security for this asset.
- In the bottom pane select the action or the user for which you want to set security and select or clear theAllowandDenyboxes accordingly. ClickHelpfor more detailed information on using the dialog box and on FactoryTalk Security.
Provide Feedback