Meaning of each action
The following table shows the meaning of each action.
This action... | Allows the user to... |
|---|---|
AssetCentre | |
CheckIn does not require MoC workflow | Turn off the Management of Change workflow when checking in selected files and binders associated with the selected asset. Select Deny box to require Management of Change workflow on check-in operation. |
CheckOut - CheckIn | Check out or check in files and binders associated with the selected asset. |
CheckOut does not require workflow | Turn off the Management of Change workflow when checking out files and binders associated with the selected asset. Select Deny box to require Management of Change workflow on check-out operation. |
Get | Get a copy of the file or files associated with the selected asset from Archive. |
Label | Apply a descriptive label to a version of a file associated with the selected asset in Archive. |
Pin | Pin a version of a file associated with the selected asset. |
Promote | Store an old version of the file as the most recent version. |
Set Store Latest Version | Specify that only the most recent version of the file associated with the selected asset should be retained. |
Set Working Folder | Set the working folder for files associated with the selected asset. |
Unblock MoC workflow | Reset the Management of Change workflow status of files and binders associated with the selected asset. |
Undo CheckOut | Undo a check-out operation for files associated with the selected asset. |
Common | |
Configure Security | Change security settings for the selected asset. |
Create Children | Add assets underneath the selected asset (only if the selected asset is a container or device-type asset). |
Delete | Delete the selected asset from the asset tree. |
Execute | This setting is not applicable in this release of FactoryTalk AssetCentre software. |
List Children | Show children of the selected asset. If a user does not have this right, they will not be able to expand the selected asset to see assets that it contains. If you set this right to Allow, also set the Read right for this asset to Allow. |
Read | Show the selected asset in the asset tree. Show the selected asset's properties. |
Write | Change the selected asset's properties. |
Provide Feedback