Options dialog box: Stratix Switch
How do I open the Options: Stratix Switch dialog box?
- SelectTools > Options.
- UnderCategoryon the left side of the dialog box, selectStratix Switch.
Use the
Options: Stratix Switch
dialog box to configure a maximum time duration in seconds for which the Allen-Bradley Stratix Switch transfers requested data to FactoryTalk AssetCentre. Depending on the complexity of your network topology, you can specify an integer from 1 through 999. The more complicated your network is, the more time it may need for the Stratix Switch to send requested information to FactoryTalk AssetCentre. The default value is 60 seconds.Provide Feedback